Mechanical Materials and Laboratory Testing Equipment
Request Information
Skip down to:
^ Back to top ^
STATIC TESTERS
Universal Static Strength Testers; Tension/Compression
Hardness Testers
- 60,000 (Baldwin)
- 300,000 (Baldwin)
^ Back to top ^
DYNAMIC TEST SYSTEMS
Hardness Testers
- Load Frames (ranging from 1000 - 300,000 lb. capacity)
- Spectrum Controlled Bearing Testers (ranging from 5000 - 100,000 lb. capacity)
- 1000 lb. Actuators
- 2500 lb. Actuator
- 5000 lb. Actuators
- 10,000 lb. Actuator
- 20,000 lb. Actuators
- 35,000 lb. Actuator
- 50,000 lb. Actuator
- 100,000 lb. Actuator
- 200,000 lb. Actuator
- 300,000 lb. Actuator
^ Back to top ^
UNIVERSAL HIGH SPEED DYNAMIC TESTERS
Mechanical or hydraulic load controlled testers operating at 10-30Hz.
High Speed Testers
- 4000 lb. (Schenk)
- 200,000 (Amsler)
^ Back to top ^
CONTROLLERS
Controls servovalves for fatigue tests.
Controller Equipment:
- MTS 407 Controllers
- MTS 458 Controllers
- Com System - 16 Channels for Multi-Channel Simulation of Field Loading
- CTM System - 16 Channels for Multi-Channel Simulation of Field Loading
- TRAC - 8 Channels for Multi- Channel Simulation of Field Testing
^ Back to top ^
THERMOMECHANICAL TEST EQUIPMENT
Equipment:
- Thermotron environmental chamber (22″ x 14″ x 16″)
There are two holes at the top and bottom for actuators. The holes are approximately 4″ in diameter and have centers 9.5" from the front of the chamber. The Controller for this chamber can maintain temperatures to ±3° F. The upper temperature limit is approximately 300° F. Low temperatures are maintained by the adiabatic expansion of gases. The gas that is used determines the lower limit. There are two additional chambers that operate in the same manner.
Equipment:
Specs:
- Hot/Wet/Cold
- Temp -100˚F to 375˚F
- Relative humidity 20-95%
- Size: 3ft. x 3ft. x 3ft.
- NOTE: Humidity is only operational between 40˚F and 185˚F
Equipment:
Specs:
- Hot/Wet/Cold
- Temp -100˚F to 375˚F
- Relative humidity 20-95%
- Size: 2ft. x 2ft. x 2ft.
- NOTE: Humidity is only operational between 40˚F and 185˚F
Equipment:
Specs:
- Hot/Cold
- Temp -100˚F to 375˚F
- Size: 4ft. x 4ft. x 4ft.
High Temperature Only Units
- ThermoTron (385˚F, 72" x 42" x 36")
- Greunberg (650˚F, 72" x 42" x 36")
High Temperature Only Units
Specs:
- Hot/Cold (No humidity)
- Temp -100˚F to 375˚F
- Size: 12" x 11" x 16"
^ Back to top ^
METALLURGICAL TESTING LAB EQUIPMENT
Hardness Testers
Equipment:
- Brinell Hardness Tester
- Superficial Scale Rockwell Testers
- Standard Rockwell Testers
- MicroHardness Testers
Optical Equipment:
Equipment:
- Optical Comparator
- Binocular Microscopes (75x) – Leica, Bausch & Lomb
- Inverted Stage Metallograph (Jenaphot)
- Scanning Electron Microscope (Zeiss EVO 500)
Other Met Testing Laboratory Equipment:
Equipment:
- Baird DV-2 Optical Emissions Spectrometer
- Metallurgical Wet Abrasive Sectioning Saws
- Band Saws
- Harshaw Salt Fog Chamber
- Alternate Emersion Tester
- Automatic Polisher for Metallurgical Specimens
- Hot Mounting Press
- Polishing and Replication Equipment:
Polymer Chemistry Lab Equipment:
Equipment:
- TA Q10 Differential Scanning Calorimeter (DSC)
- Nicolet Impact 420 Fourier Transform Infrared Spectrometer (FTIR)
- Kayness Melt Flow Plastometer
- Thermolyne Muffle Furnaces
- Shore A Durometer Hardness Tester
- Shore D Durometer Hardness Tester
- Barcol Hardness Tester
- Mettler AT261 Delta Range Balance
- Accumet AB-15 ph Meter
- Nikon Transmission Microscope
- Autocut Mod 1140 Microtome
Electordynamic Vibration Testers
Equipment:
- Vibration Research Corporation (VRC) Controllers
With capabilities to control, measure and perform the following tests:
- Sine Frequency Sweep with constant displacement or acceleration
- Random with frequency weighted power spectral density
- Shock with half-sine, haversine, triangular or saw-tooth pulses
- Shock Response Spectrum (SRS) with frequency weighted spectral density
- Playback of recorded acceleration using replication of data collected in the field.
- Sine on Random to simulate vibration generated by rotating machinery with multiple vibration tones(orders)
- Mode identification using resonance search, transmissibility and stroboscopy
- Modal analysis
Additional Electordynamic Vibration Testers
Equipment:
- Ling Amplifier 30KVA
- Unholz-Dickie Amplifier 20KVA
- Dynamic Solutions Amplifier 6KVA
- 17,000 lbf Shaker
- 6000 lb. Ling Shakers (All modified for longer stroke)
- 4000 lb. Unholtz-Dickie Shaker
- 1200 lb. M-B Shaker
- 1200 lb M-B Amplifier
^ Back to top ^
CHAIN TESTERS (4-SQUARE TESTERS)
Four square tests are done on one of five machines with the following specifications:
Description |
Max. Load (Lbs.) |
Max. Speed (RPM) |
Min. Center Distance (in.) |
Max. Center Distance (in.) |
Motor (HP) |
Large wear tester |
15,000 |
500 |
28 |
41 |
30 |
Small wear tester |
3,500 7,500 (oil) |
3,000 (grease) |
14 |
24 |
15 |
Medium wear tester |
3,500 |
2,500 |
21 |
33 |
15 |
Corrosion wear tester |
6,000 |
40 to 1,000 |
22 |
36 |
15 |
Small leaf chain tester |
5,000 |
4,800 |
7.5 |
12 |
25 |
*ACA Tester |
60,000 (60)
25,000 (40) |
300 |
40 |
70 |
75 |
* This tester is currently in storage and not instantly available for use
** Dependent on chain size.
^ Back to top ^
BEARING OSCILLATION TESTERS
Equipment:
Specs:
- Load capacity: Radial loads of 20,000 – 100,000 lbs.
- Temp -50˚F to 450˚F
- Oscillation angles: 2˚-150˚
- Speeds: 10-350 CPM
These testers are generally used to perform standard capacity testing to evaluate changes in material, design, and manufacturing processing.
4-Servohydraulic Testers
Four testers capable of applying constant, variable, or programmed sequences of load and motion are available. Push-pull loading of up to 100,000 lbs. can be accommodated while the included oscillation angle can vary from 1º to 60º within temperatures ranging from -50º to 1000ºF. The cyclic rate depends on the load and oscillation angle, but up to 1200 CPM may be applied at 1º oscillation. These testers are utilized to perform specialized complex load-motion spectra for qualification testing and simulation of actual in-service conditions of aerospace bearings.
Industrial Bearing Test Stands
Mounted bearing life test capacity testers: Four 4-bearing per shaft test stations w/flood oil lubrication. These are typically used for standard rolling contact fatigue life testing. The flood oil system has the capability to cool and filter (10 micron) the supply oil. These testers run tests at fixed speeds and loads but can be changed manually (drive sprockets) during the test setup. Load per bearing up to 8,000 lbs.; speeds range from 1000 to 2400 rpm.
Abrasive/seal test: One 4-bearing per shaft test station. This rig has a self contained sand elevator and dispersing apparatus. These testers run tests at fixed speeds and loads but can be changed manually (drive sprockets) during the test setup. Loads per bearing up to 3,000 lbs; speeds range 100 to 1800 rpm.
Grease lubed temperature rise/shaft mount evaluation: One 4-bearing per shaft test station. These testers run tests at fixed speeds and loads but can be changed manually (drive sprockets) during the test setup. Loads per bearing up to 3,000 lbs; speeds range 100 to 1800 rpm.
Cylindrical/unmounted bearing life test capacity testers: Four 4-bearing per shaft test stations w/flood oil lubrication. These testers have a variable speed motor/Controller and the test beds were built with a potential add-on servohydraulic loading capability.
These testers have a variable speed motor/Controller but loads again are fixed. Loads per bearing up to 6,000 lbs; speeds range from 1000 to 3600 rpm.
^ Back to top ^
COUPLING TESTERS
Equipment:
Specs:
- Two parallel shaft gearboxes (approx 3:1 ratios) in a back-to-back configuration
- Speed and torque can be varied independently from each other
- (4) test couplings can be misaligned to a preset value during test
- Torque is applied by a rotating hydraulic actuator connected to one of the gearboxes
CAPACITY
- Continuous running: 2,197 ft-lb @ 5462 RPM (high speed side)
- 6,667 ft-lb @ 1800 RPM (low speed side)
INTERMITTENT DUTY
- 5,493 ft-lb @ 5462 RPM (high speed side)
- 16,667 ft-lb @ 1800 RPM (low speed side)
Equipment:
- Low Capacity 4-Square (Wrapflex) Tester
Specs:
- Lower torque load/misalignment testing of smaller couplings such as Wrapflex
- High speed shaft torque capacity is 889 lb-in at 1750 rpm
- Low speed shaft torque capacity is 4,445 lb-in at 350 rpm
- Motor is 5 HP @ 1750 rpm VFD
- Speed and torque cannot be adjusted while running
- Torque is mechanically adjusted through a rigid flange-style coupling in which the two halves are rotated with respect to each other
- Currently have (3) test stations on high-speed side and no stations on low-speed side
- Plate size is 4' x 11'
Equipment:
- Pneumatic Reverse Torque Fatigue Tester
Specs:
- Used for new material and process evaluation and quality control for Omega production
- Primarily tests E20 size only, but can test E4 if necessary
- 1,840 in-lb. capacity
- Applies cyclic torque by a double-acting pneumatic cylinder attached to a moment arm
- Load (and torque) cycles in a square wave profile from (+) load to (-) load
Equipment:
Specs:
- Used for new material and process evaluation and quality control for Omega production
- 83% energy savings
- Tests Omega E4 couplings at 3X catalog torque, 3600 rpm, and under misalignment
- 1,650 in-lb. capacity
Equipment:
Specs:
- Used for new material and process evaluation and quality control for Omega production
- Tests Omega E4 couplings at 3X catalog torque, 3600 rpm, and under misalignment
- Four-square configuration with (3) test stations
- Torque capacity is 2,000 in-lb
Equipment:
Specs:
- Used for new material and process evaluation and quality control for Omega production
- Tests Omega E4 couplings at 5 degrees angular misalignment but near zero torque
- 0 Torque; 3 stations 1900 rpm; 3 stations 2960 rpm
Equipment:
Specs:
- Used to test Omega and Viva couplings for shear strength of the cap screws and/or elastomeric element
- Electric motor spins test coupling to 3600 rpm
- Motor is disengaged and a pneumatic brake is actuated
- Loads as high as 45,000 in-lb have been measured
Equipment:
- Hydraulic Reverse Torque Fatigue Tester
Specs:
- Built for testing disc couplings and larger Omega couplings in cyclic torque, 100,000-120,000 in-lb max
- 0 rpm
Equipment:
- 250 HP Water-Cooled Eddy Current Dynamometer
Specs:
- Developed to test magnetic couplings; and fluid coupling starting characteristics.
- 250 HP
- Two motors available and can be changed out within 1 day; 1800 RPM and 3600 RPM
Equipment:
- Small Reverse Torque Tester
Specs:
- (2) 6,000 lb-in (left side) and (2) 30,000 lb-in fixed displacement reverse torsion fatigue testers
- Used for torque/deflection/stiffness, axial thrust, torsional fatigue and ultimate strength testing
- Converted to pneumatic cylinder for load application to generate torque
- Bed Plate size is 6'8" x 10'
Equipment:
- Large Reverse Torque Tester
Specs:
- (1) 150,000 lb-in fixed displacement reverse torsion fatigue tester
- Used for torque/deflection/stiffness, torsional fatigue and ultimate strength testing
- Motor: 20 HP @ 1745 rpm and 20 or 25 HP @ 1800 rpm
- Could be converted to servo-hydraulic control and loading
- Bed Plate size is 7'10" x 15'
Equipment:
- Back to Back Coupling Test Stand
Specs:
- High torque load/misalignment 4-square tester
- High speed shaft torque capacity: 54,000 lb-in at 1750 rpm
- Low speed shaft torque capacity: 98,000 lb-in at 960 rpm
- Motor is 150 HP @ 1750 rpm, but needs to be converted to a variable speed drive. Torque within tester can be varied while running by axially displacing the pinion in one of the “Y" units
- Plate size is 7' x 20'.
- NOTE: Torque can only be applied in one direction due to damaged gear in drive end reducer
Equipment:
- Steelflex 4-Square Testers
Specs:
- This test stand was originally built by Falk to be a gear tester
- The smaller four-square was referred to as the “3.7785 Gear Tester"
- The larger four-square was referred to as the “7.5 Gear Tester". 1090T10
- “7.5" and “3.7785" refer to the center distance
Equipment:
Specs:
- Test coupling is on the low speed shaft
- Low speed side rotates at 596 rpm
- Gear ratio is 3:1
- Maximum torque capacity is not known. However, a 1060T grid coupling is rated to 6,050 in-lb and is currently installed
- Torque is measured by a strain gage system that is on the high speed side. High speed side is not used for testing but could develop 1800 rpm and 2000 in-lb.
- Shaft ends going into the 1060T grid coupling are Ø1.7500/1.7495 with (1) 3/8 key. (ref. Falk drawings EX1548 and EX3202)
Equipment:
Specs:
- Test coupling is on the low speed shaft
- Low speed side rotates at (unknown) rpm
- Gear ratio is 3.44:1
- Maximum torque capacity is not known. However, a 1090T grid coupling is rated to 33,000 in-lb and is currently installed
- Torque is measured by a strain gage system that is on the high speed side. High speed side is not used for testing but could develop 1800 rpm and 9593 in-lb.
- Shaft ends going into the 1060T grid coupling are Ø3.5650/3.5645 with (1) 7/8 key. (ref. Falk drawings 237573 and 320768)
Equipment:
Specs:
- 20,000 rpm zero torque spin tester. (9 in. max radius)
- Maximum speed dependent on mass and balance characteristics of unit being tested. (2,500 rpm minimum)
^ Back to top ^
FLAT-TOP TESTERS
Controller Equipment:
- L-Conveyor Testers (50-500 fpm/500 lb. corner tension)
- Jerk-Fatigue Stand (0-1500 lb, 0.2-
- Hz; 4 stations)
- Jerk-Fatigue Stand (0-2000 lb, 0.2-
- Hz; 4 stations)
- S-Conveyor (70-500 fpm/70-600 lb. corner tension)
- SS Wear Strip Tester (6 lanes; 20- 600 fpm/10-50 lbf, top load)
^ Back to top ^
NEW at Rexnord Innovation Services
Rexnord Innovation Center has provided innovation services and testing services for decades. Our experienced staff keeps abreast of the most cutting edge technologies. Here are a few of the latest additions to our innovation arsenal:
Tribometer
A linear reciprocating pin‐on‐disk (POD) tribometer was recently acquired to help advance RIC engineer's understanding of friction and wear phenomena. The tribometer can quantitatively assess the coefficient of friction between two sliding surfaces and can be used as a high throughput testing tool to screen the friction coefficient or wear rate between many different materials.
SEM
The Scanning Electron Microscope (SEM) was primarily purchased to perform failure analysis on components and to support the growth of the RIC's analytical metrology capabilities. The SEM can magnify from 30x up to 300,000x, and has a 100x wider depth of field (the distance between objects that are in focus) than traditional light optical microscopes. The SEM is also able to detect differences in composition between adjacent regions and quantify the chemical composition of the samples.
FTIR
The Fourier Transform Infra‐Red (FTIR) spectroscopy Equipment: at the Rexnord Innovation Center was recently upgraded to provide new capabilities. This new instrument can examine the chemical structure of materials such as polymers, coatings, composites, elastomers, lubricants and solvents. This proves to be a very useful tool for vendor validation, competitive analysis, and contamination analysis.
ProJet® 3500 HD Max Professional 3D Printer
To better support clients with product development issues, the Rexnord Innovation Center has acquired a state of the art 3D printer capable of rendering of high quality, functional parts / models which are ideal for functional testing.
This machine has a net build volume of 11.75" x 7.3" x 8", and is capable of using different materials when the application dictates.