Top 2 Causes of Bearing Failure

|
Accurately diagnosing potential bearing failures ahead of time is important to preventing unexpected downtime and increased maintenance costs. These key bearing-failure causes account for the majority of individual bearing failures. By taking note of these causes, and taking the necessary preventative measures, there is the potential to extend a bearing's service life, reduce unscheduled downtime, and increase overall workplace productivity. These are the most common causes of premature bearing failure:

1) Lubrication and Contamination

Blog Content Image

Lubrication is a critical part of a bearing’s lifecycle. Lubricate the bearing too little, and the lubrication can become contaminated and cause excessive wear and possibly heat up, which will lead to premature bearing failure. Lubricating too much can cause a bearing to overheat, but only when the speeds are high. In general applications it is very difficult to over lubricate. Choosing the correct seal will also help with lubrication and contamination failures. Choosing the correct seal and finding the correct frequency and amount of lubrication for your bearing is critical to preventing unplanned downtime.

2) Improper Installation

While it may seem like common sense, standard wear and tear is one of the leading causes of bearing failure. Eventually all bearings fail due to wear, however, excessive load, vibration or force can cause a bearing to wear out long before it should. Most of this excess force is caused by improper installation. If you don't install your bearing properly, and to the OEM's specifications, you are setting your bearing up for failure. Following the OEM's installation instructions can be the difference between successful operation of your application.

Although there are numerous symptoms, each bearing failure typically results from a combination of issues, and not just a single cause. Be aware of the issues that prompt bearing failure, look for the warning signs, and take the preventative measures needed to keep your bearings operating at or above peak performance for as long as possible.

For more information on Rexnord Bearings such as installation manuals, videos and product specifications, click here.

How to Properly Lubricate your Bearing Tip Sheet

To learn more about bearing failure, and how to prevent it, download our How to Properly Lubricate a Bearing Tip Sheet.

Download

Mark   Czubak

Mark Czubak is a Principal Engineer with the Rexnord Bearing business. He has spent nearly 40 years with Rexnord where he has managed all facets of engineering, including application, design and manufacturing, giving him a cradle to grave knowledge of mounted roller bearings. With this experience, Mark shares his passion and knowledge through bearing training, application assistance and installation. “Bearings are overlooked for the more expensive components of the system, but a bearing failure can cause just as much downtime as any other component so choose your bearings wisely, and save time and money.”